nvt4857uk datasheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nvt4857uk datasheet

995 Views
larice
Contributor I

Looking at the NVT4857UK datasheet I'm missing timing specifications for anything else except 1.2 -> 1.8.

I'd like to verify timing for a usage case with vcca=1.8 and vccb=3.3 as well as vccb=1.8

Further I'd expect the datasheet to talk a bit about requirements for the

  "automatic direction control". There surely will be some requirements to make this work properly,

  maximum length of signal reflections, transition times or something like this.

Best Regards,

Tags (1)
0 Kudos
Reply
2 Replies

921 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

I understand your concern and you are right about the missing information in the datasheet, however, I checked with the applications team and product engineers team of this device and we do not have more data than the one is in the datasheet already.

 

NVT4857UK is compliant to SD Physical Spec version 3.01, so, you can use that as reference for the timings of 1.8V and 3.3V.

Regards,

Jose

0 Kudos
Reply

921 Views
larice
Contributor I

Thank You for the warm words, and for having checked.

I will have to live with the status quo.

Best Regards,

Robert

0 Kudos
Reply