nvt4857uk datasheet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

nvt4857uk datasheet

929件の閲覧回数
larice
Contributor I

Looking at the NVT4857UK datasheet I'm missing timing specifications for anything else except 1.2 -> 1.8.

I'd like to verify timing for a usage case with vcca=1.8 and vccb=3.3 as well as vccb=1.8

Further I'd expect the datasheet to talk a bit about requirements for the

  "automatic direction control". There surely will be some requirements to make this work properly,

  maximum length of signal reflections, transition times or something like this.

Best Regards,

タグ(1)
0 件の賞賛
返信
2 返答(返信)

855件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

I understand your concern and you are right about the missing information in the datasheet, however, I checked with the applications team and product engineers team of this device and we do not have more data than the one is in the datasheet already.

 

NVT4857UK is compliant to SD Physical Spec version 3.01, so, you can use that as reference for the timings of 1.8V and 3.3V.

Regards,

Jose

0 件の賞賛
返信

855件の閲覧回数
larice
Contributor I

Thank You for the warm words, and for having checked.

I will have to live with the status quo.

Best Regards,

Robert

0 件の賞賛
返信