Hello,
I'm having trouble trying to write to a sensor register using the mc13224V, the configuration of the i2c module *seems* to be fine, but when trying to write the application hangs, I have read similar threads in the forum and have not find an answer, I must say I'm just beggining working with the mc13224V, and I tested the sensor communication using the open libmc1322x and it worked, so the sensor wiring, pull-up resistors, etc have been tested using the same development board.
The sensor's 7-bit slave address is 0x39, the operation I'm using for testing is powering the sensor by writting 0x03 to the register at 0x00, maybe I'm misunderstanding the I2c_SendData instruction and sintaxis.
The logic analyzer doesn't show anything (not even the clock source), the error message I receive from the sendData instruction is gI2cErrModuleBusy_c, but that's strange because between the configuration stage and the actual sendData attempt I'm waiting 1-2 seconds.
Am I missing a magic enable or something?
Below is my test code, I appreciate any hints or pointers.
Cheers,
--Antonio
/*********************** CONFIGURE ************************************************/
void foo init_sensor(){
I2cErr_t error;
/* Creates structures */
I2cConfig_t i2cConfig;
/* Clear and initialize */
I2c_Init();
/* Configure pins for I2C (functional mode 1) */
Gpio_SetPinFunction(gGpioPin12_c, gGpioAlternate1Mode_c);
Gpio_SetPinFunction(gGpioPin13_c, gGpioAlternate1Mode_c);
/* Enables the I2C module */
error = I2c_Enable();
if(error != gI2cErrNoError_c){
error_led();
return;
}
/* Assign the interrupt handle */
IntAssignHandler(gI2cInt_c, (IntHandlerFunc_t)&I2c_Isr);
ITC_SetPriority(gI2cInt_c, gItcNormalPriority_c);
ITC_EnableInterrupt(gI2cInt_c);
/* I2C configuration */
i2cConfig.slaveAddress = 0x01; // Our slave address, not used in Master mode
i2cConfig.freqDivider = 0x20; // X/160, 150KHz for 24Mhz peripheral clock
i2cConfig.saplingRate = 0x10; // Digital filter sample rate (default)
i2cConfig.i2cInterruptEn = TRUE;
i2cConfig.i2cBroadcastEn = FALSE;
error = I2c_SetConfig(&i2cConfig);
if(error != gI2cErrNoError_c){
error_led();
return;
}
/* Set callback functions */
error = I2c_SetCallbackFunction(&SensorCallback);
if(error != gI2cErrNoError_c){
error_led();
return;
}
return;
}
/*********************** TEST COMMAND ************************************************/
void foo_test(){
I2cErr_t error;
uint8_t cmd_buffer[] = {0x00,0x03};
error = I2c_SendData(0x39, &cmd_buffer[0], 2, gI2cMstrReleaseBus_c);
if(error != gI2cErrNoError_c){
error_led();
return;
}
void SensorCallback(uint16_t transfBytesNo, uint16_t status){
test_led_on();
}
Solved! Go to Solution.
Nevermind, I got it working... besides having external pull-up resistors, magic trick was enabling the internal pull-up resistors, and from there figuring out that instead of writting to 0x39 I should write to 0x72.
In case anyone bumps with this, hope to help.
Nevermind, I got it working... besides having external pull-up resistors, magic trick was enabling the internal pull-up resistors, and from there figuring out that instead of writting to 0x39 I should write to 0x72.
In case anyone bumps with this, hope to help.