Hi guys,
ltib for MPC8318E RDB is failing on my Ubuntu 9.10.
vishal@shrek:~/Freescale/ltib-mpc8313erdb-20081222$ ./ltib -c+ [ -n -a ! -f config/platform/mpc8313erdb/.config ]+ [ -n ]+ cd config/platform/mpc8313erdb+ mconf main.lkcsh: mconf: not foundDied at ./ltib line 2689.traceback: main::ltib_config:2689 main::pre_build_checks:1288 main:495Started: Sun Feb 20 22:36:17 2011Ended: Sun Feb 20 22:36:17 2011Elapsed: 0 secondsBuild FailedExiting on error or interruptvishal@shrek:~/Freescale/ltib-mpc8313erdb-20081222$
The error part of the host_config.log is as follows
Executing(--clean): /bin/sh -e /home/vishal/Freescale/ltib-mpc8313erdb-20081222/tmp/rpm-tmp.N9pRXE+ umask 022+ cd /tmp/rpm-vishal/BUILD+ rm -rf rpm-4.0.4+ exit 0Build time for rpm-fs: 157 secondserror: cannot open Name index using db3 - No such file or directory (2)error: cannot open Name index using db3 - No such file or directory (2)sudo rpm --root / --dbpath /tmp/rpm-vishal/rpmdb -e --allmatches --nodeps --define '_tmppath /home/vishal/Freescale/ltib-mpc8313erdb-20081222/tmp' rpm-fs 2>/dev/nullsudo rpm --root / --dbpath /tmp/rpm-vishal/rpmdb --ignorearch -ivh --force --nodeps --excludedocs --define '_tmppath /home/vishal/Freescale/ltib-mpc8313erdb-20081222/tmp' /tmp/rpm-vishal/RPMS/i686/rpm-fs-4.0.4-1.i686.rpmrpm: please use alien to install rpm packages on Debian, if you are really sure use --force-debian switch. See README.Debian for more details.sudo /opt/freescale/ltib/usr/bin/rpm --root / --dbpath /opt/freescale/ltib/var/lib/rpm -Uv --justdb --notriggers --noscripts --nodeps /tmp/rpm-vishal/RPMS/i686/rpm-fs-4.0.4-1.i686.rpmsudo: /opt/freescale/ltib/usr/bin/rpm: command not foundProcessing platform: Host support packages============================================using /home/vishal/Freescale/ltib-mpc8313erdb-20081222/config/platform/host/ltib.preconfigProcessing: fake-provides===========================Build path taken because: no prebuilt rpm,
I have attached the host_config logfile.
Please suggest what package do I need to install / remove to get ltib installed.
Can you try (K)Ubuntu 8.04? Linux BSP for MPC8313E is proven to work on this KUbuntu version, and we don't officially support Ubuntu 9.x and higher.
By the way, you can create a formal service request to our support team on https://www.freescale.com/webapp/servicerequest.create_SR.framework for LTIB issues. You can get faster response from them.
Hi Vishal,
Can you share with me how you have resolved this mconf error?
At present I am facing same error with my ubuntu 9 version.
Error :-
Can't exec "mconf": No such file or directory at /u/users/srilak/L3.0.35_12.09.01_GA_source/ltib_cvs_latest/bin/Ltibutils.pm line 1011.
exec: mconf /u/users/srilak/L3.0.35_12.09.01_GA_source/ltib_cvs_latest/config/main.lkc: No such file or directory at /u/users/srilak/L3.0.35_12.09.01_GA_source/ltib_cvs_latest/bin/Ltibutils.pm line 1011.
Regards,
Srilakshmi
are u still facing the problem or is it solved? it says sudo command not found! have u installed sudo in ur linux?