ltib complaing of missing config file after ltib -m distclean

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib complaing of missing config file after ltib -m distclean

1,462 Views
LGJ
Contributor I

Real newbie question here. I just installed and built the BSP that came with my 8315E RDB. Everything was fine, then I typed the ltib -m distclean command that is supposed to clean everything out except the shared directories. Anyway, according to the user manual I should just have to type "./ltib" and it should reconfigure and build everything again. When I try that, however, the blue configuration screen pops up asking for the config file. I leave the name ".config" to use the default and the config screen complains that it can not find it. Can someone tell me how do get this system back to factory default without reinstalling?

 

Thanks,

Leo

Tags (1)
0 Kudos
Reply
1 Reply

624 Views
gleb_itech
Contributor I
make --configure
0 Kudos
Reply