ltib complaing of missing config file after ltib -m distclean

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ltib complaing of missing config file after ltib -m distclean

1,473 次查看
LGJ
Contributor I

Real newbie question here. I just installed and built the BSP that came with my 8315E RDB. Everything was fine, then I typed the ltib -m distclean command that is supposed to clean everything out except the shared directories. Anyway, according to the user manual I should just have to type "./ltib" and it should reconfigure and build everything again. When I try that, however, the blue configuration screen pops up asking for the config file. I leave the name ".config" to use the default and the config screen complains that it can not find it. Can someone tell me how do get this system back to factory default without reinstalling?

 

Thanks,

Leo

标记 (1)
0 项奖励
回复
1 回复

635 次查看
gleb_itech
Contributor I
make --configure
0 项奖励
回复