ls1012A quad enable bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1012A quad enable bit

517件の閲覧回数
yogeshddave
Contributor II

Dear All,

I am using LS1012A-FRWY and it has Winbond SPI flash. I want to set quad-enable bit (QE bit) of status register2 to 1. can somebody guide how to achieve this?

I also want to know which QE bit number of status register 2 is applicable for winbond like devices. Moreover it will be helpful if someone knows If there is any way to check the status of this Quad Enable bit?

Thanks in advance.!

0 件の賞賛
返信
1 返信

430件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following update from the AE team.

This information should be available in the Winbond SPI flash datasheet/manual. Customers can use similar steps to those used for writing on the flash. However, to write to the flash internal registers, the opcode for the command will be different (which should be available in the flash documents).

0 件の賞賛
返信