I tried to build Linux for imx6ull14x14evk with fsl-imx-wayland distro of Ubuntu 20.04 (WSL2) which I already allocated 16GB of RAM and 4 cores processor. after running: bitbake imx-image-core, the kernel fetch process seems working fine.
but after 30%, the error occurs, and it starts to fetch from the mirror source but not successfully.
How can I solve this problem? If possible, step to perform manual download is also appreciated.
已解决! 转到解答。
After observing the error message: I found out that the build system expected the file name: github.com.nxp-imx.linux.git. So I do as follow:
1. git clone -b lf-5.15.y https://github.com/nxp-imx/linux-imx.git to any dir is ok
2. copy the clone dir to download-dir/git2 by change the name to github.com.nxp-imx.linux.git
3. create. done by touch github.com.nxp-imx.linux.git. done
4. run bitbake -c cleanall
5. run bitbake imx-core-image
Now it working.
But one thing I notice from error message, seem the build recipe have the error on the path when perform the mirror do_fetch because download path on my machine is : /home/megamama/imx-yocto-bsp/downloads/git2/ but it use /home/megamama/imx-yocto-bsp/downloads//git2/ (double //)
Hi @Harvey021
Thanks for sharing helpful steps.
here, I'm also facing the same issue :
ERROR: linux-imx-5.15.71+gitAUTOINC+50912be386-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/linux-imx.git;protocol=https;branch=lf-5.15.y')
Later i followed your steps given above for manual method downloading of repo (git clone -b lf-5.15.y https://github.com/nxp-imx/linux-imx.gitinto) into git2 folder.
1. github.com.nxp-imx.linux.git -> copied
2. github.com.nxp-imx.linux.git.done -> copied
but the next command : bitbake -c cleanall its not working in my case
also after that i tried with calixto-systems@calixtosystems-HP-Notebook:~/rpr/yocto/cs_nxp_yocto/calixto-nxp-yocto/build_imx$ bitbake -c cleanall imx-image-multimedia & clean world commands despite the same issue.
So suggest me if any other method to resolve this issue
Thanks in advance.
Regards,
Ravikumar
This is just a possible (not sure it can work) step that you can try:
1. set up yocto build system so that download dir is outside of build dir
2. copy your git clone to download/git2
3. delete sstate-cache, tmp and cache in build dir
4. run bitbake core-image-minimal again
Other alternative option:
1. clone kernel repo
2. modify your kernel-recipes to fetch from local git repo instead
Hi,
I'd have a doubt that the fetch issue is related to your local network.
GitHub - nxp-imx/linux-imx at lf-5.15.y here you can have a try manual download.
git clone https://github.com/nxp-imx/linux-imx.git which should be put in <path to build>/downloads and then touch a copy of it with ext ".done"
Regards
Harvey
Thank you for your response!
But I am still new to Yocto and I have some questions related to manually configuring the kernel.
1. If I do git clone, do I need to checkout to a specific branch If-5.15.y?
2. As I check in the download directory, I see all fetch files are compression with ext . tar.gz. Do I need to compress my kernel file after clone?
3. If I need to compress, what name should I give to this compress file?, so yocto build system can find it
After observing the error message: I found out that the build system expected the file name: github.com.nxp-imx.linux.git. So I do as follow:
1. git clone -b lf-5.15.y https://github.com/nxp-imx/linux-imx.git to any dir is ok
2. copy the clone dir to download-dir/git2 by change the name to github.com.nxp-imx.linux.git
3. create. done by touch github.com.nxp-imx.linux.git. done
4. run bitbake -c cleanall
5. run bitbake imx-core-image
Now it working.
But one thing I notice from error message, seem the build recipe have the error on the path when perform the mirror do_fetch because download path on my machine is : /home/megamama/imx-yocto-bsp/downloads/git2/ but it use /home/megamama/imx-yocto-bsp/downloads//git2/ (double //)