Hi
I'm developing a project with imx-21 arm processor in company where I work (Wise Indústria de Telecomunicações from Brazil). I want implemented video decoder in board with imx21, I use hantro decoder, emma player (emma-binary-mx21-2.0) and linux kernel 2.4.20.
I need compile the package emma-binary-mx21-2.0, especially emma-play, because I need to increase the variable rtp.size in emma_play.c. But to recompile the source code, I need file config.mak, included in emma_play makefile, because the package emma-binary-mx21-2.0, don't contains this file.
How do I do to get the file config.mak of emma-binary-mx21-2.0???
I use ltib (BSP version TO3.2), the emma-binary is package from Ltib. I already try recompile using Ltib, but I don't get sucess, because Ltib don't make the new executables.
How do I do to recompile emma-binary???
Thanks
Message Edited by MarcelWISE on
2008-05-15 06:14 PM