Hi guys.
I am checking camera preview with gst-launch-1.0. I already checked camera preview with mxc_v4l2_overlay app embeded in rootfs. below is command used:
./mxc_v4l2_overlay.out -iw 720 -ih 576 -ow 640 -oh 480 -m 3 -di /dev/video0 fg
I have checked USB camera and it worked with below command:
gst-launch-1.0 v4l2src device=/dev/video2 ! 'video/x-raw, width=640,height=480' ! imxv4l2sink
but, when i use gst-launch-1.0 for previewing of camera, It doesn't work. below is command used:
1.gst-launch-1.0 v4l2src device=/dev/video0 ! 'video/x-raw, format=(string)UYVY,width=640,height=480,framerate=(fraction)30/1' ! autovideosink
2.gst-launch-1.0 v4l2src device=/dev/video0 ! autovideosink
Why that error happens? I want to know to fix that error for previewing of camera in application specially for opencv
* linux ver. 4.14.98-2.0.0
since you use PAL camera, you should video/x-raw, format=(string)UYVY,width=720,height=576, I don't know what you mean doesn't work, pls share the logfile to check , maybe you can try like 'gst-launch-1.0 videotestsrc ! 'video/x-raw, format=(string)UYVY,width=720,height=576,framerate=25/1' ! imxvideoconvert_ipu ! 'video/x-raw, format=RGB16' ! mfw_v4lsink'
Hi Joanxie,
1. below is logfile when i used "gst-launch-1.0 v4l2src device=/dev/video0 ! 'video/x-raw,width=720, height=756, framerate=25/1' ! videoconvert ! imxv4l2sink
: In MVC: mxc_v4l_ioctl 80045626
case VIDIOC_G_INPUT
Plpeline is live and does not neeIn MVC:mxc_v4l_ioctl PREROLL...
Setting pipeline tIn MVC: mxc_v4l_do_ioctl c0405602 PLAYING...
In MVC:mxc_v4l_ioctl
New clock: GstSystemClock
In MVC: mxc_v4l_do_ioctl c02c563a
case VIDIOC_CROPCAP
ERROR: from element /GstPipeline: In MVC: mxc_v4l_close
pipeline0/GstV4l2Src:v4l2src0: Inmxc_v4l_close: release resource
internal data stream erro.
Additi MVC: In mxc_free_frame_buffer
onal debug info:
../../../../gitIn MVC:mxc_free_frames
/libs/gst/base/gstbasesrc.c(3055): gst_base_src_loop (): /GstPipeline0/GstV4l2Src:v4l2src0:
streaming stopped, reason not-negotiated (-4)
2. below is command's logfile which you recommanded:
/# gst-launch-1.0 videotestsrc ! 'video/x-raw, format=(string)UYVY,width=720,height=576,framerate=25/1' ! imxvideoconvert_ipu ! 'video/x-raw, format=RGB16' ! mfw_v4lsink
WARNING: errorneous pipeline: no element "mfw_v4lsink"
refer to the 4.14.98 user guide,
7.3.8 Camera preview
This example displays what the camera sees. It is only available on platforms with a camera.
$GSTL v4l2src ! 'video/x-raw, format=(string)$FORMAT,
width=$WIDTH, height=$HEIGHT, framerate=(fraction)30/1'
! v4l2sink
Camera preview example:
$GSTL v4l2src device=/dev/video1 ! 'video/x-raw,
format=(string)UYVY,width=640,height=480,framerate=(fraction)30/1'
! autovideosink
Parameter comments:
• Get the camera support format and resolution using gst-inspect-1.0 v4l2src.
• Set caps filter according to the camera's supported capabilities if the user needs other format or resolution.
• Ensure that the right caps filter has been set, which also needs to be supported by v4l2sink
Hi Joanxie,
gst-launch-1.0 v4l2src device=/dev/video0 ! 'video/x-raw,width=720, height=756, framerate=25/1' ! videoconvert ! imxv4l2sink
-> I added "format=(string) UYVY" in above command but, didn't work
Hi Joanxie,
1. "./mxc_v4l2_overlay.out -iw 720 -ih 576 -ow 640 -oh 480 -m 3 -di /dev/video0 fg"
-> Yes, It works,
2. "gst-launch-1.0 videotestsrc ! 'video/x-raw, format=(string)UYVY, width=720,height=576,framerate=25/1, interlace-mode=(string)progressive' ! imxv4l2sink"
the above command works, but when change src from videotessrc to v4l2src, it doesn't work.
And, I have checked below command:
3. "gst-device-monitor-1.0" and results are:
(gst-device-monitor-1.0:645): GIn MVC:mxc_v4l_ioctl
Streamer-CRITICAL **: In MVC: mxc_v4l_do_ioctl c02c563a
gst_element_message_full_with_details: assertion 'GST_IS_ELEMENT(element)' failed
In MVC:mxc_v4l_close
mxc_v4l_close: release resource
MVC: In mxc_free_frame_buf
Invalid crop param: crop.w0, crop.h=0
mxc_v4l2_output v4l2_out: filed format:4 not supported yet!
Invalid crop param: crop.w0, crop.h=0
mxc_v4l2_output v4l2_out: filed format:4 not supported yet!
......
Hi Joanxie,
Thank for your answering. Could you give me favor?
Please let me know "v4l2-ctl --all -d 0" in your side.
My "v4l2-ctl --all -d 0" is :
================================
Video input: 0 (CSI IC MEM: ok)
Video output: 0 (DISP3 BG)
Video Standard = 0x000000ff
PAL-B/B1/G/H/I/D/D1/K
Format Video Capture:
Width/Height : 288/352
Pixel Format : 'Yu12"
Field : Any
Bytes per Line : 432
------------------------------------
Format Video Overlay:
Left/Top : 0/0
Width/Height : 160/160
-------------------------------------
Framebuffer Format:
capability : Extern Overlay
Flags : Overlay Matches Capture/Output Size
Width : 0
Height : 0
----------------------------------
Crop Capability Video Capture :
Bounds : Left 0, Top 0, Width 720, Height 625
Default : Left 0, Top 0, Width 720, Height 625
---------------------
this is mine:
Driver Info:
Driver name : mxc_v4l2
Card type :
Bus info :
Driver version : 0.1.11
Capabilities : 0x05000005
Video Capture
Video Overlay
Read/Write
Streaming
Video input : 0 (CSI IC MEM: ok)
Video output: 0 (DISP3 BG)
Video Standard = 0x00000000
Format Video Capture:
Width/Height : 288/352
Pixel Format : 'YU12'
Field : Any
Bytes per Line : 432
Size Image : 152064
Colorspace : Default
Transfer Function : Default (maps to Rec. 709)
YCbCr/HSV Encoding: Default (maps to ITU-R 601)
Quantization : Default (maps to Limited Range)
Format Video Overlay:
Left/Top : 0/0
Width/Height: 160/160
Field : Any
Chroma Key : 0x00000000
Global Alpha: 0x00
Clip Count : 0
Clip Bitmap : No
Framebuffer Format:
Capability : Extern Overlay
Flags : Overlay Matches Capture/Output Size
Width : 0
Height : 0
Pixel Format : ''
Crop Capability Video Capture:
Bounds : Left 0, Top 0, Width 640, Height 480
Default : Left 0, Top 0, Width 640, Height 480
Pixel Aspect: 0/0
Crop: Left 0, Top 0, Width 640, Height 480
Streaming Parameters Video Capture:
Capabilities : timeperframe
Frames per second: 30.000 (30/1)
Read buffers : 0