blhost(2.6.7) error check.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

blhost(2.6.7) error check.

Jump to solution
833 Views
StephenYeh
Contributor III

Hi Sir,

Would you help us to check the blhost(2.6.7) error  feedback(0x4 & 0x2714)?

What are the error message about 0x4 Invalid Argument Error and 0x2714 (No response packet from target device)?blhost.JPG

 

0 Kudos
Reply
1 Solution
804 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @StephenYeh 

Why are you using the hex 0x0020?, and after the -- flash-erase-all you have a 9, maybe this is giving you an error, are you using an LPC Link 2 to programming? Which MCU are you using? is it a custom board?

View solution in original post

0 Kudos
Reply
3 Replies
803 Views
StephenYeh
Contributor III

Hi Sir

This is the special part, we have fixed this bug. Thanks.

blhost_2.6.7\bin\win>blhost.exe -u 0x1FC9,0x0020 -- get-property 1

Inject command 'get-property'

Response status = 0 (0x0) Success.

Response word 1 = 1258488064 (0x4b030100)

Current Version = K3.1.0

 

805 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @StephenYeh 

Why are you using the hex 0x0020?, and after the -- flash-erase-all you have a 9, maybe this is giving you an error, are you using an LPC Link 2 to programming? Which MCU are you using? is it a custom board?

0 Kudos
Reply
789 Views
StephenYeh
Contributor III
The R?610 serial downlaod mode with HID, the PID/VID is the 20h. And the bootrom version is K3.1.0 .
0 Kudos
Reply