any difference between SJA1124AHG/0Z and SJA1124AHG/1Z?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

any difference between SJA1124AHG/0Z and SJA1124AHG/1Z?

284件の閲覧回数
sebastian-uchman
Contributor I

Does anyone know the difference between this two?

0 件の賞賛
返信
1 返信

270件の閲覧回数
pavla_hajna
NXP TechSupport
NXP TechSupport

Dear Sebastian Uchman,

Design changes SJA1124xHG/0 and SJA1124xHG/1
Two IP blocks were adjusted:
• The under voltage VIO timer
− The under-voltage recovery time of this timer was increased to match the MFIO start-up time
As a result, the MFIO output is well defined
• The main state machine
− The boot time was increased to match the MFIO start-up time.
Both changes were only changes in digital.

Important note - The new SJA1124AHG/1Z and SJA1124AHG/0Z are pin-to-pin compatible and software compatible (drop-in replacements).

Have a nice day. Best regards

Pavla

 

0 件の賞賛
返信