Hi,
Wifi is not working in Android 10 on imx8mq EVK board. From logcat I can see Timeout on wlan driver when trying to enable wifi.
12-23 12:36:54.004 3341 3341 E WifiHAL : Timed out waiting on Driver ready ...
12-23 12:36:54.004 3341 3341 E android.hardware.wifi@1.0-service: Timed out awaiting driver ready
12-23 12:36:54.004 3341 3341 E android.hardware.wifi@1.0-service: Failed to start legacy HAL: TIMED_OUT
The timeout is due to /sys/class/net/wlan0 not found.
Traced in file: hardware/qcom/wlan/qcwcn/wifi_hal/wifi_hal.cpp
wifi_error wifi_wait_for_driver_ready(void)
{
// This function will wait to make sure basic client netdev is created
// Function times out after 10 seconds
int count = (POLL_DRIVER_MAX_TIME_MS * 1000) / POLL_DRIVER_DURATION_US;
FILE *fd;
do {
if ((fd = fopen("/sys/class/net/wlan0", "r")) != NULL) {
fclose(fd);
return WIFI_SUCCESS;
}
usleep(POLL_DRIVER_DURATION_US);
} while(--count > 0);
ALOGE("Timed out wating on Driver ready ... ");
return WIFI_ERROR_TIMED_OUT;
}
I tried with pre-build images as well from nxp and observation the same behaviour.
Please help me to resolve this.
Regards,
Sunitha
Hello,
Just to say that I am working on this problem with the internal team.
Best regards,
Diego.
Hello,
I apologize for the delay,
Hi, which wifi module on your evk board are you using? 1CQ or 1CX?
Best regards,
Diego.
Hi Diego,
We checked on our evk board and found that Wifi module 1CQ is being used.
Regards,
Sunitha
Hi Diego,
Any update on this?
Regards,
Sunitha