Who can give me some explain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Who can give me some explain

2,789 Views
CaoJason
Contributor I
Hello:
     Who can give me some explain about this:lis r29,0xfff00000@h.I cann't know well about 0xfff00000@h. also the 0xfff00000@l
0 Kudos
Reply
9 Replies

1,211 Views
CrasyCat
Specialist III
Hello
 
This is explained in the {Install}\Help\PDF\Assembler Reference.pdf (Where {Install} refers to your CodeWarrior installation directory).
Take a look at chapter "Assembly Language Syntax" section "Symbols" -> "Labels".
 
There is a table there called "Relocatable label expressions", which explains all this.
 
I hope this helps.
 
CrasyCat
0 Kudos
Reply

1,211 Views
CaoJason
Contributor I
Thanks Cat.
I get it.
Also can you give me some file to explain the details about MPC564EVB link files:such as MPC564EVB_RAM.lcf
MEMORY {
 ram : org = 0xFFF00000
 rom : org = 0xFFD00000
 
// ram : org = 0x00C02000
// rom : org = 0xFFF00000 // desired ROM address
}
 
FORCEACTIVE { gInterruptVectorTable, __reset, __ext_int, __decr, __machine_check }
SECTIONS {
// GROUP : { .intvec : {}
// } > vectors
 GROUP : {
  .reset : {}
  .intvec : {}
  .init : {}
  .text (TEXT) : {}
  .rodata (CONST) : {
   *(.rdata)
   *(.rodata)
  }
  .ctors : {}
  .dtors : {}
  extab : {}
  extabindex : {}
 } > ram  
// } > rom  
 
 GROUP : {
  .data : {}
  .sdata : {}
  .sbss : {}
  .sdata2 : {}
  .sbss2 : {}
  .bss : {}
  .PPC.EMB.sdata0 : {}
  .PPC.EMB.sbss0 : {}  
 } > ram
 // The dummy section is just a placeholder.  The linker automatically
 // generates an address for it in the ROM image, which tells us
 // where the end of the ROM image is.
 .dummy ALIGN(64): {}
 
}
Thanks and best regards!
Jason
0 Kudos
Reply

1,211 Views
CrasyCat
Specialist III
Hello
 
Sorry but what is the question here?
 
If you are looking for some documentation about linker command file syntax, look in
{Install}\Help\PDF\Power Arch Build Tools Reference.pdf. There is a chapter "Linker" in there, with a whole section "Linker Command File syntax" explaining the syntax of the .lcf file.
 
I would recommend reading the whole chapter as the sections before provides some good set of information as well.
 
If that was not the question, can you please be more specific.
 
CrasyCat
0 Kudos
Reply

1,211 Views
CaoJason
Contributor I

Hi cat:

   I have another questions :

         1).the MPC564 have BR0~BR3 and OR0~OR3 registers.What's usage about these registers?

         2). Is the address of internal RAM and  onboard(exterior) RAM,and internal FLash and onboard(exterior) Flash fixed,that's defined by vendor(the address of which is given out in Reference Manual),or it can programmed by value in the BR0~BR3 and OR0~OR3?

Sorry,Cat ,I ask many questions in one tittle,do I need to new another topic?

Cao Jason



Message Edited by CaoJason on 2008-09-16 11:35 AM
0 Kudos
Reply

1,211 Views
CrasyCat
Specialist III
Hello
 
These are configuration registers that are described in the "MPC561/MPC563 Reference Manual".
Take a look at section 10 memory Controller there.
 
The reference manual can be downloaded from the Freescale  Web site,
 
CrasyCat
0 Kudos
Reply

1,211 Views
CaoJason
Contributor I
sorry,Cat,I have read though this chapter,but I still have these doubt
0 Kudos
Reply

1,211 Views
CrasyCat
Specialist III
Hello
 
I am not a hardware person, so I do not have much more information on that.
 
I will let someone with hardware knowledge answer that.
 
Alternatively you can submit a service request for that.

Click here to submit a service request.

CrasyCat
0 Kudos
Reply

1,211 Views
CaoJason
Contributor I
Thanks Cat,I'm waiting
0 Kudos
Reply

1,211 Views
CaoJason
Contributor I
Hi Cat:
    Thanks,I have understood the link file.
Cao Jason
0 Kudos
Reply