Which SSD flash driver for SPC564B74L7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which SSD flash driver for SPC564B74L7

889件の閲覧回数
kloetpatra
Contributor I

Hi!

Which SSD flash driver do I need for device SPC564B74L7 ?

At MPC564|32 Bit Microcontroller (MCU)|Freescale there is no download for the flash driver. However I need one for programming flash through JTAG Nexus Interface.

Is it possible to use the C90FL_JDP_SSD http://cache.freescale.com/files/microcontrollers/software/device_drivers/C90FL_SM_JDP_FLASH_SSD_DEV... ?

In Nexus Programming Spec http://cache.freescale.com/files/32bit/doc/app_note/AN4365.pdf there are only following devices listed with the same core type. But It seems for specific devices there are specific ssd drivers, so I am not sure which one to use, or if there's a MPC564B74 specific one too?

MPC deviceFreescale SSD flash driverCore type
MPC564xL
C90FL_JDP_SSDe200z4
MPC564xA
MPC5644A_C90FL_JDP_SSDe200z4
0 件の賞賛
返信
1 返信

586件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

SPC564B74L7 is device from ST, so you should ask rather ST :smileyhappy:

http://www.stmicroelectronics.com.cn/web/en/catalog/tools/PF258748

Compatible device from Freescale is this one:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC564xB-C

And SSD drivers can be downloaded here (can be found on the page above, tab "Software & Tools"):

http://www.freescale.com/files/soft_dev_tools/software/device_drivers/MPC56XX_C90LC_JDP_SSD_100_DEVD...

Regards,

Lukas

0 件の賞賛
返信