What is the sampling rate of the Mc33772?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the sampling rate of the Mc33772?

Jump to solution
387 Views
jingfang
Contributor IV

What is the sampling rate of the Mc33772?

0 Kudos
Reply
1 Solution
383 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jingfang,

ADC2 and ADC1-A,B clocking frequency is 6 MHz.

Regarding the sampling frequency, in normal mode, it is driven by the MCU. When a start of conversion command is sent on SPI or TPL bus, then the device will sample all CTx and ANx channels.

In cyclic acquisition mode, it depends on the content of the CYCLIC_TIMER bits in the SYS_CFG1 register.

Best regards,

Tomas

View solution in original post

1 Reply
384 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jingfang,

ADC2 and ADC1-A,B clocking frequency is 6 MHz.

Regarding the sampling frequency, in normal mode, it is driven by the MCU. When a start of conversion command is sent on SPI or TPL bus, then the device will sample all CTx and ANx channels.

In cyclic acquisition mode, it depends on the content of the CYCLIC_TIMER bits in the SYS_CFG1 register.

Best regards,

Tomas