What is the sampling rate of the Mc33772?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the sampling rate of the Mc33772?

跳至解决方案
420 次查看
jingfang
Contributor IV

What is the sampling rate of the Mc33772?

0 项奖励
回复
1 解答
416 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jingfang,

ADC2 and ADC1-A,B clocking frequency is 6 MHz.

Regarding the sampling frequency, in normal mode, it is driven by the MCU. When a start of conversion command is sent on SPI or TPL bus, then the device will sample all CTx and ANx channels.

In cyclic acquisition mode, it depends on the content of the CYCLIC_TIMER bits in the SYS_CFG1 register.

Best regards,

Tomas

在原帖中查看解决方案

1 回复
417 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jingfang,

ADC2 and ADC1-A,B clocking frequency is 6 MHz.

Regarding the sampling frequency, in normal mode, it is driven by the MCU. When a start of conversion command is sent on SPI or TPL bus, then the device will sample all CTx and ANx channels.

In cyclic acquisition mode, it depends on the content of the CYCLIC_TIMER bits in the SYS_CFG1 register.

Best regards,

Tomas