What is the sampling rate of the Mc33772?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the sampling rate of the Mc33772?

Jump to solution
374 Views
jingfang
Contributor IV

What is the sampling rate of the Mc33772?

0 Kudos
1 Solution
370 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jingfang,

ADC2 and ADC1-A,B clocking frequency is 6 MHz.

Regarding the sampling frequency, in normal mode, it is driven by the MCU. When a start of conversion command is sent on SPI or TPL bus, then the device will sample all CTx and ANx channels.

In cyclic acquisition mode, it depends on the content of the CYCLIC_TIMER bits in the SYS_CFG1 register.

Best regards,

Tomas

View solution in original post

1 Reply
371 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jingfang,

ADC2 and ADC1-A,B clocking frequency is 6 MHz.

Regarding the sampling frequency, in normal mode, it is driven by the MCU. When a start of conversion command is sent on SPI or TPL bus, then the device will sample all CTx and ANx channels.

In cyclic acquisition mode, it depends on the content of the CYCLIC_TIMER bits in the SYS_CFG1 register.

Best regards,

Tomas