What is the sampling rate of the Mc33772?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the sampling rate of the Mc33772?

ソリューションへジャンプ
528件の閲覧回数
jingfang
Contributor IV

What is the sampling rate of the Mc33772?

0 件の賞賛
返信
1 解決策
524件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jingfang,

ADC2 and ADC1-A,B clocking frequency is 6 MHz.

Regarding the sampling frequency, in normal mode, it is driven by the MCU. When a start of conversion command is sent on SPI or TPL bus, then the device will sample all CTx and ANx channels.

In cyclic acquisition mode, it depends on the content of the CYCLIC_TIMER bits in the SYS_CFG1 register.

Best regards,

Tomas

元の投稿で解決策を見る

1 返信
525件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jingfang,

ADC2 and ADC1-A,B clocking frequency is 6 MHz.

Regarding the sampling frequency, in normal mode, it is driven by the MCU. When a start of conversion command is sent on SPI or TPL bus, then the device will sample all CTx and ANx channels.

In cyclic acquisition mode, it depends on the content of the CYCLIC_TIMER bits in the SYS_CFG1 register.

Best regards,

Tomas