A number of different firmware versions (F1 to F6) are available for this chip, but nowhere are the specific details of each version described.
Which version to choose?
Also please send me the accompanying documents AN11128 (Programming Guide), AN11133 (Flash-over-AUX Utility User's Guide), and AN11134 (DPDC Utility User's Guide) as well as the software tool that is mentioned for setting up registers.
Kind regards Kasper
解決済! 解決策の投稿を見る。
Hello Kasper,
All the app notes as well as firmware updates including implemented changes are available on this website. I would recommend using the latest version (F6).
I hope it helps.
Best regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
If anyone has DisplayPort flickering issues, you should try using the DPCD tool. You will probably see symbol errors. DPCD registers provide a lot of information including link settings and match the DisplayPort spec from VESA. And don't use Fast Link Training use Full Link Training. We learned the hard way.
The link for the firmware and the description off them is no more valid. May you post it again ?
The link provided on your response is no longer valid. Where can I find this tool?
Just wondering about the firmware utility from the above link.
I scan it with Microsoft Security Essentials it sees it as a trojan.
Is this considered normal or is it something I shall worry about?
Hello Kasper,
All the app notes as well as firmware updates including implemented changes are available on this website. I would recommend using the latest version (F6).
I hope it helps.
Best regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
We also need actual firmware and tools because of flickering 17.3 inch FHD displaymodule.
PTN3460 we have got with final hardware has an development version on it.
Please can you provide an active link again.
Thanks
Best Regards
Stefan
Hello Stefan,
did the firmware update fix your problem with the flickering display? If so, which firmware version did you update to? We are connecting a FullHD Display to a DP source via a PTN3460BS and have problems with flickering displays too.
Thanks and best regards
Max
Hello Max,
yes it works well, we could not see any flickering. To check this, we took a camera recording changes on the screen.
The old firmware was F2 and we updated to the new F6.
Best Regards
Stefan
Hi Stefan.
I just sent you a PM.
I have the files, and if you mail me I will send them to you.
My adress is in the private message. BTW, we had to do some hacking to the Linux core in order to force the link eDP link training to occur.
I suppose a non-trained eDP link could be the root cause of the image flickering since it could be a boundary condition signal integrity wise. We had no image at all before enforcing the training, but maybe our matching of the differential lines were more 'off' than yours is.
I can supply some more info on how we solved this. It was our Linux guy that did it, so I have to ask him
Hello Kasper,
sorry for my late answer. Thanks a lot for your help and for the firmware. It works well.
We found version F2 in the chips and we installed version F6.
No flickering again, we are happy with this and our customer also.
Our problem ist solved.
Thanks and best Regards
Stefan
We are using the Apalis TK1 module from Toradex. The following link is a description from Toradex on the issue:
linux-toradex.git - Linux kernel for Apalis and Colibri modules
Our Linux guy wrote the following when he checked in the altered Linux file thingy:
I have been debugging the driver a bit to see how the link training worked. According to the standard, there are 2 parameters to adjust: Voltage Swing (values 0.4, 0.6, 0.8, 1.2) and Pre-emphasis (values 0dB, 3.5dB, 6dB, 9.5dB). The driver initiates the link training, but it is the sink (i.e. the PTN3460 chip) that chooses which parameter values to use. The link training has 2 phases: Clock recovery and channel equalization. The clock recovery would always succeed with the lowest settings, but the channel equalization would not. The PTN3460 would then step wise instruct the driver to turn up the voltage swing parameter – but the link training would not succeed. After trying all 4 values of the voltage swing, I would expect the PTN3460 chip to reset the voltage swing and increase pre-emphasis – but it did not. Instead it bailed out and to the driver, the next step would be to decrease the pixel clock. The pixel clock could, however, not be lowered because it would then not be able to carry the full data rate (on the 2 channels), and hence the whole procedure was aborted. What I did, was to hack the driver use pre-emphasis 3.5dB and then it succeed (with voltage swing 0.4). This seems to work every time and seems to be stable. There are 2 things I do not quite like about this solution: 1) Not all combinations of Voltage Swing and Pre-emphasis are allowed. When increasing Pre-emphasis one step, then one step (the largest) is removed from the allowed Voltage Swing. By just forcing pre-emphasis to 3.5dB (without the chip knowing), we could end up in a situation where the chip requests and illegal voltage swing, and there is no logic in the driver (right now) to catch this. 2) I must admit I don’t quite understand the driver fully. For instance it has internally two arrays of 4 elements – one for Voltage Swing and one for Pre-emphasis. It seems, though, that all values in the arrays are set to the same value. And why would you need an array for *each* parameter? You only need to send one value to the driver!? Basically, not understanding the driver fully, it makes me wonder whether it is the chip that fails to adjust the pre-emphasis, or if it is the driver that fails to recognize instructions from the chip to adjust the pre-emphasis. But right now, I think we are happy that it seems our hardware works :-)