I have been told that the bfu725f/N1 can be used in 30GHz DRO(checked). i want to use it design a 26GHz DRO, but i m not sure the mex model of this transistor can be used in 26GHz. i check the data sheet , but not metion the mex model is build to which frequency.
MEX model is not valid at these frequencies.
Use S-parameters for a 26GHz application.
Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------