WCT1013A FlexCAN drive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WCT1013A FlexCAN drive

Jump to solution
1,101 Views
2194133213
Contributor I

There is a problem with the FlexCAN driver for WCT1013A.Where is the FlexCAN in the MCU controller the same IP driver?     

thank you

0 Kudos
Reply
1 Solution
1,010 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is FlexCAN example with FlexCAN driver, pls refer to it.

BR

Xiangjun Rong

View solution in original post

0 Kudos
Reply
3 Replies
1,010 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The Kinetis K family uses the FlexCAN IP which is the same as the CAN module of MC56F84xxx/MC56F82xxx.

The Kinetis has peripheral driver package SDK, you can download the SDK package from the link:

Welcome | MCUXpresso SDK Builder 

The SDK package can be based on MCUXpresso, Keil, IAR tools and Windows OS.

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply
1,010 Views
2194133213
Contributor I

Hi,xiangjun.rong

   I have not found that the FlexCAN in a certain MCU controller is an IP chip. Could you please provide a model of MCU and a link to download the complete routines of MCU?

thank you

0 Kudos
Reply
1,011 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is FlexCAN example with FlexCAN driver, pls refer to it.

BR

Xiangjun Rong

0 Kudos
Reply