Voltage Rating of Capacitors on SJA1105SMBEVM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Voltage Rating of Capacitors on SJA1105SMBEVM

跳至解决方案
1,291 次查看
ivan_kenetics
Contributor II

I would like to find out the voltage rating of some of the capacitors mounted on SJA1105SMBEVM as the BOM is not available.

Can someone help to advise the voltage rating of the capacitors for the below location? Those capacitors are used in the 100Base-T1 connection.

C174, C175 (0.1uF)

C427 (4700pF).

 

 

标签 (1)
0 项奖励
回复
1 解答
1,274 次查看
guoweisun
NXP TechSupport
NXP TechSupport

In the AH1706 of TJA1101 app note:

AC coupling
In Fig 11 AC coupling is realized by using 100nF coupling capacitors forming a high-pass
filter together with the termination of 50Ohm for each line.

The tolerance of the capacitors shall be within ±10% with max rating ≥50V.

在原帖中查看解决方案

3 回复数
1,277 次查看
guoweisun
NXP TechSupport
NXP TechSupport

The tolerance of the capacitors shall be within ±10% with max rating ≥50V.

0 项奖励
回复
1,275 次查看
guoweisun
NXP TechSupport
NXP TechSupport

In the AH1706 of TJA1101 app note:

AC coupling
In Fig 11 AC coupling is realized by using 100nF coupling capacitors forming a high-pass
filter together with the termination of 50Ohm for each line.

The tolerance of the capacitors shall be within ±10% with max rating ≥50V.

1,275 次查看
ivan_kenetics
Contributor II

Would appreciate if NXP can advise the exact manufacturer part number or voltage rating of those cap. Open Alliance system implementation did mentioned that those capacitors should be => 50V for 12V system and =>100V for 24V system. But on TJA1101 Board, the 4700pF capacitor voltage rating is only 10V.

 

0 项奖励
回复