Hi Ajnas,
OTP programming determines the power-up sequence for the regulators. When the power-up sequence is finished, the main state machine is in Normal_M mode, which is the application running mode with all the regulators on. Then all regulators can be individually disabled using corresponding bits (LDOxDIS, BUCKxDIS, BOOSTDIS, VPREDIS) in the M_REG_CTRL1 register (Table 84 in the datasheet).
Best regards,
Tomas