Using PTN5150 in DFM only what then about VBUS_DET?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using PTN5150 in DFM only what then about VBUS_DET?

跳至解决方案
1,162 次查看
thomaskofoedhan
Contributor III

I want to use the PTN5150 for a DFM application only with 3A capability, but what should I do with the VBUS_DET pin?

Thomas

标记 (2)
1 解答
1,027 次查看
thomaskofoedhan
Contributor III

Thank you Jose, for the answer. Clear and precise 

在原帖中查看解决方案

0 项奖励
2 回复数
1,027 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

When the PTN5110 controller is configured as a DFP mode application only, the VBUS_DET pin can be left unconnected.

Regards,

Jose

1,028 次查看
thomaskofoedhan
Contributor III

Thank you Jose, for the answer. Clear and precise 

0 项奖励