Unable to Run Examples in NXP Vision Toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to Run Examples in NXP Vision Toolbox

454件の閲覧回数
abijithb1
Contributor I

Hello all,

I experimenting with the SBC S32V234 board and I'm not able to run the examples in the toolbox on the board. For the example face detection, on running the code, the command window shows:

>> run_application
FFmpeg library already installed
Warning: Support for the RTW.HWDeviceRegistry class will be removed in a future release. For information
about upgrading data definitions for your hardware, see Upgrade Data Definitions for Hardware Devices.
> In RTW.HWDeviceRegistry
In rtwTargetInfo
In coder.targetreg.internal.TargetRegistry/refresh
In coder.targetreg.internal/TargetRegistry/refreshToolchain
In coder.make.internal.getToolchainInfos (line
In coder.make.internal.guicallback.getToolchains (line 9)
In coder.internal.setToolchainOptions
In coder/Hardware/addedToConfig
In nxpvt_codegen
In nxpvt_runner/Run (line 63)
In run_application (line 7)
Warning: Support for the RTW.HWDeviceRegistry class will be removed in a future release. For information
about upgrading data definitions for your hardware, see Upgrade Data Definitions for Hardware Devices.
> In RTW.HWDeviceRegistry
In rtwTargetInfo
In coder.targetreg.internal.TargetRegistry/refresh
In coder.targetreg.internal/TargetRegistry/refreshCrl
In coder.internal.getTfl
In isTargetLangSupportedByTFL
In isTargetLangSupportedByTFL
In isTargetLangSupportedByTFL
In rtwprivate (line 16)
In coder.internal.compile
In emlckernel
In emlckernel
In emlckernel
In emlckernel
In emlcprivate
In codegen
In nxpvt_codegen
In nxpvt_runner/Run (line 63)
In run_application (line 7)
Warning: Support for the RTW.HWDeviceRegistry class will be removed in a future release. For information
about upgrading data definitions for your hardware, see Upgrade Data Definitions for Hardware Devices.
> In RTW.HWDeviceRegistry
In rtwTargetInfo
In coder.targetreg.internal.TargetRegistry/refresh
In coder.internal.getTflTableList
In RTW/resolveTflName
In emcBuildRTW
In emcGenMakefileAndBuild
In emcGenMakefileAndBuild
In emcBuildTarget
In emlcprivate
In coder.internal.compile
In emlckernel
In emlckernel
In emlckernel
In emlckernel
In emlcprivate
In codegen
In nxpvt_codegen
In nxpvt_runner/Run (line 63)
In run_application (line 7)
Compilation suppressed: generating code only.
Warning: Treating [] as double [1 x 0] to match later assignments.
More information
Warning in ==> filter_objects Line: 3 Column: 5
Code generation successful (with warnings): View report
Warning: Directory already exists.
> In nxpvt_build
In nxpvt_make
In nxpvt_codegen
In nxpvt_runner/Run (line 63)
In run_application (line 7)

C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\examples\advanced\face_detection\codegen\exe\face_detection>SET PATH=C:/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/../compilers/gcc-6.3.1-linaro-Earmv7-eabi/i686-mingw32/bin;C:\Program Files\MATLAB\R2020b\bin\win64;C:\Program Files\MATLAB\R2020b\toolbox\imaq\imaqextern\drivers\win64\genicam\GenICam_V3_1_0\bin\Win64_x64;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\lib\oal;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\lib\opencv;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\target;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;C:\windows\System32\OpenSSH\;C:\Program Files\NVIDIA Corporation\NVIDIA NvDLISR;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\WINDOWS\System32\OpenSSH\;C:\Program Files\Ricardo\bin;C:\Program Files (x86)\Windows Kits\8.1\Windows Performance Toolkit\;C:\Program Files\MATLAB\R2020b\runtime\win64;C:\Program Files\MATLAB\R2020b\bin;C:\Program Files\MATLAB\R2019b\runtime\win64;C:\Program Files\MATLAB\R2019b\bin;C:\Program Files\PuTTY\;C:\Users\abiji\AppData\Local\Microsoft\WindowsApps;

C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\examples\advanced\face_detection\codegen\exe\face_detection>SET PATH=C:/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/../compilers/gcc-6.3.1-linaro-Xarmv8-linux/i686-mingw32/bin;C:/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/../compilers/gcc-6.3.1-linaro-Earmv7-eabi/i686-mingw32/bin;C:\Program Files\MATLAB\R2020b\bin\win64;C:\Program Files\MATLAB\R2020b\toolbox\imaq\imaqextern\drivers\win64\genicam\GenICam_V3_1_0\bin\Win64_x64;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\lib\oal;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\lib\opencv;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\target;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;C:\windows\System32\OpenSSH\;C:\Program Files\NVIDIA Corporation\NVIDIA NvDLISR;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\WINDOWS\System32\OpenSSH\;C:\Program Files\Ricardo\bin;C:\Program Files (x86)\Windows Kits\8.1\Windows Performance Toolkit\;C:\Program Files\MATLAB\R2020b\runtime\win64;C:\Program Files\MATLAB\R2020b\bin;C:\Program Files\MATLAB\R2019b\runtime\win64;C:\Program Files\MATLAB\R2019b\bin;C:\Program Files\PuTTY\;C:\Users\abiji\AppData\Local\Microsoft\WindowsApps;

C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\examples\advanced\face_detection\codegen\exe\face_detection>SET PATH=C:/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/../msys32/mingw32/bin;C:/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/../msys32/usr/bin;C:/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/../msys32/mingw64/bin;C:/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/../compilers/gcc-6.3.1-linaro-Xarmv8-linux/i686-mingw32/bin;C:/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/../compilers/gcc-6.3.1-linaro-Earmv7-eabi/i686-mingw32/bin;C:\Program Files\MATLAB\R2020b\bin\win64;C:\Program Files\MATLAB\R2020b\toolbox\imaq\imaqextern\drivers\win64\genicam\GenICam_V3_1_0\bin\Win64_x64;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\lib\oal;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\lib\opencv;C:\Users\abiji\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_Vision_Toolbox_for_S32V234(2)\internals\target;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;C:\windows\System32\OpenSSH\;C:\Program Files\NVIDIA Corporation\NVIDIA NvDLISR;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\WINDOWS\System32\OpenSSH\;C:\Program Files\Ricardo\bin;C:\Program Files (x86)\Windows Kits\8.1\Windows Performance Toolkit\;C:\Program Files\MATLAB\R2020b\runtime\win64;C:\Program Files\MATLAB\R2020b\bin;C:\Program Files\MATLAB\R2019b\runtime\win64;C:\Program Files\MATLAB\R2019b\bin;C:\Program Files\PuTTY\;C:\Users\abiji\AppData\Local\Microsoft\WindowsApps;
Current SDK ROOT is /c/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk
/bin/sh: -c: line 2: syntax error near unexpected token `('
/bin/sh: -c: line 2: ` make -C /c/Users/abiji/AppData/Roaming/MathWorks/MATLAB Add-Ons/Toolboxes/NXP_Vision_Toolbox_for_S32V234(2)/examples/advanced/face_detection/codegen/exe/face_detection/build-v234ce-gnu-linux-o/../graphs/build-apu-nxp-sa-d SUB_EXTERN_DEP=0 allsubsub; \'
make: *** [/c/NXP/VisionSDK_S32V2_RTM_1_7_0/s32v234_sdk/build/nbuild/platforms/coordinator.mk:115: allsub] Error 1
Warning: Cannot deploy on target. Compilation failed..
> In nxpvt_codegen
In nxpvt_runner/Run (line 63)
In run_application (line 7)
>>

 

 

I would appreciate any help to solve this issue.

Thanks,

Abijith

0 件の賞賛
返信
0 返答(返信)