UJA1079 SBC first reset after power on

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UJA1079 SBC first reset after power on

Jump to solution
854 Views
szblaci
Contributor III

Hello!

I am using UJA1079 SBC in my application (for LIN, WDG and power supply).

If I ignore the WDG update then I have SBC reset periodically in every 128 ms (default NWP) which is the expected reaction. 

But somehow right after the power on ("cold reset") the first reset cycle takes about 260 ms. Only the first one then the others come nicely in every 128 ms.  

Is this the intended behavior or something can be wrong with my hardware (PCB)?  

0 Kudos
1 Solution
841 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi László,

I am not so familiar with this older SBC UJA1079, but the attached AH1002 gives the description below.

Capture 3.1.2.JPG

So after system reset, the watchdog configuration must be executed in 256ms before it starts, I guess.

Best regards,

Tomas

View solution in original post

0 Kudos
2 Replies
842 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi László,

I am not so familiar with this older SBC UJA1079, but the attached AH1002 gives the description below.

Capture 3.1.2.JPG

So after system reset, the watchdog configuration must be executed in 256ms before it starts, I guess.

Best regards,

Tomas

0 Kudos
839 Views
szblaci
Contributor III

Hello Tomas,

Thanks a lot for the fast replay and the specification! It seems to be very detailed and helpful. 

regards

Laszlo

 

0 Kudos