TagWriter WiFi action fails via tag

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TagWriter WiFi action fails via tag

864 次查看
frank_fuchs
Contributor I

Hi,

we have a customer hotspot. When using the path through the Android settings/WiFi to connect to this hotspot - everything is fine. A captive Portal mini browser site pops up,aso

But when we use a tag to connect (with the same hotspot of course ;-) it fails. Cannot receive the IP address....

The tag is written by choosing the HotSpot from Android OS.

Any ideas?

Frank

0 项奖励
回复
5 回复数

674 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Frank Fuchs,

I am going to answer both of your threads here if that is ok for you, 

I have tested this with my phone and an NTAG213  this is what I stored and tested with my colleagues phones and it worked:

pastedImage_1.pngpastedImage_2.png

please confirm your wifi information also the phones you are using to test this.

as much information you can provide please let me know.

BR

Jonathan

0 项奖励
回复

674 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

also please let me know what reader are you using if it is the one on the phone with the tagwritter.

BR

Jonathan

0 项奖励
回复

674 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hello Frank Fuchs,

Hope you are doing great, I think that what Paulina asked is about what tag are you using, so we can replicate te problem or explain the correct procedure in case this works for us.

BR

 

Jonathan

0 项奖励
回复

674 次查看
frank_fuchs
Contributor I

Hello,

sorry for my late reply - I've been in vacation. 

The Tag I have used is a

"NFC Sticker, 22mm, NTAG 213, 180 Bytes, white"

from the NFC-tag-shop.de 

NFC Sticker Circus, 22 mm, NTAG 213, 180 Byte, weiß | NFC Sticker weiß & schwarz | NFC Aufkleber | N... 

hope you have an idea :-)

best

Frank

0 项奖励
回复

674 次查看
lisettelozano
NXP Employee
NXP Employee

Hello Frank, 

Could you please provide the NXP part number? 

Paulina

0 项奖励
回复