TRK-MPC5604P ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TRK-MPC5604P ADC

Jump to solution
850 Views
simbasoft
Contributor II

Hello,

We are working on a new development project based on MPC5604P MCU. We are using TRK-MPC5604P Evaluation board developed by P&E Microcomputer Systems. I'm trying to run the example code provided in Freescale Application Note  AN2865: (Section 22 ADC: Software Trigger, Continuous Scan) to experiment with the ADC functions. It is already the third day that I'm trying however, no matter what I did the ADC refuses to run. The conversion starts but  never completes. I was wondering whether anybody had already used that example code given in the AN2865 and can help me finding what is wrong.

Thank you in advance.

simbasoft

Here are the values of ADC0MCR and the ADC0MSR registers.

===============================================

ADC0MCR = 0x21000000

Bit Field Values:

    OWREN               bits[ 31:31 ] = 0    Discarded

    WLSIDE               bits[ 30:30 ] = 0    Right-aligned

    MODE                  bits[ 29:29 ] = 1    Scan Mode

    EDGLEV              bits[ 28:28 ] = 0    Ext. trigger on edge

    TRGEN                 bits[ 27:27 ] = 0    Disabled

    EDGE                   bits[ 26:26 ] = 0    Low level/Falling edge

    XSTRTEN            bits[ 25:25 ] = 0    Disabled

    NSTART               bits[ 24:24 ] = 1    Starts chain or scan conv

    Not Implemented  bits[ 23:23 ] = 0

    JTRGEN               bits[ 22:22 ] = 0    Disabled

    JEDGE                 bits[ 21:21 ] = 0    Falling edge

    JSTART                bits[ 20:20 ] = 0    No effect

    Not Implemented bits[ 19:18 ] = 0

    CTUEN                bits[ 17:17 ] = 0    Disabled

    Not Implemented bits[ 16:9  ] = 0

    ADCLKSEL           bits[  8:8  ] = 0    clkfreq=ipgclk freq/2

    ABORTCHAIN      bits[  7:7  ] = 0    Does not abort

    ABORT                bits[  6:6  ] = 0    Does not abort

    ACKO                  bits[  5:5  ] = 0    Disabled

    Not Implemented bits[  4:1  ] = 0

    PWDN                 bits[  0:0  ] = 0    Normal operation

===============================================

ADC0MSR = 0x1000804

Bit Field Values:

    Not Implemented  bits[ 31:25 ] = 0

    NSTART                bits[ 24:24 ] = 1    Conv. occurring

    JABORT                bits[ 23:23 ] = 0    New injected conv. started

    Not Implemented   bits[ 22:21 ] = 0

    JSTART                 bits[ 20:20 ] = 0    Inj. conv. not occurring

    Not Implemented   bits[ 19:17 ] = 0

    CTUSTART           bits[ 16:16 ] = 0    CTU conv. not occurring

    CHADDR              bits[ 15:9  ] = 4

    Not Implemented  bits[  8:6  ] = 0

    ACKO                   bits[  5:5  ] = 0    Disabled

    Not Implemented  bits[  4:3  ] = 0

    ADCSTATUS        bits[  2:0  ] = 4    Sample

Tags (2)
1 Solution
488 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure  the ADC is powered, J21 5V jumper should be placed.

BTW there is simple example showing ADC usage on TRK board on the https://community.freescale.com/docs/DOC-99861.

Regards,

Petr

View solution in original post

1 Reply
489 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure  the ADC is powered, J21 5V jumper should be placed.

BTW there is simple example showing ADC usage on TRK board on the https://community.freescale.com/docs/DOC-99861.

Regards,

Petr