This simple example shows the ADC setting for the scan mode and usage of Trimmer on TRK-MPC5604P board.
Use Trimmer to dim the LED1.
Regards,
Petr
********************************************************************************
* Detailed Description:
*
* ADC testing and usage of Trimmer on TRK board
*
* ------------------------------------------------------------------------------
* Test HW: TRK-MPC5604P
* Maskset: 0M36W
* Target : internal_RAM
* Terminal: no
* Fsys: 64 MHz with 8 MHz XOSC reference
* EVB connection:
*
* Use Trimmer to dim the LED1
*
* NOTE! Be sure the ADC is powered, J21 5V jumper ON
*
********************************************************************************
Hello PetrS,
Thank you for the quick response. The problem was as simple as powering the ADC - i.e. setting J21 jumper ON.
Do you know whether there are similar examples
1- for a simple FlexPWM ?
2- using the eTimers as Quadrature Decoders?
Thank you in advance.