After configuring a specific frame message for wake-up in TJA1145, the first frame of the sent message can be awakened when it is a specific frame. If the first frame of the sent message is not a specific frame and the second frame is a specific frame, it cannot be awakened. Does a specific frame necessarily require the first frame to be sent during wake-up?
Hi,
I would recommend you taking a close look at the attached AH1203 (especially Chapter 4) and AH1309.
I believe that using those two documents you will be able to better understand the selective wake-up functionality and implement it on the TJA1145.
BRs, Tomas