TJA1145 SPI communication failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1145 SPI communication failure

1,774件の閲覧回数
空心木头_mm
Contributor I

Hello :

      I am using the can transceiver TJA1145T,and I can not get the right response when I send a 0xfd to it,I am sure I have the right connection among the pins,when I monitored the SDO pin of the TJA1145T,  I found it copy the information I send to it from the pin SDI sometimes,why could this happen ?Can anyone help me?

best regrads!

0 件の賞賛
3 返答(返信)

1,229件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Mengmeng,

Do you have an oscilloscope to check if the timing and format of the SPI message is correct? 

A very common problem is that timing parameters are violated, so please make sure everything is in accordance with the following specs:

pastedImage_2.png

pastedImage_3.png

Best regards,

Tomas

0 件の賞賛

1,229件の閲覧回数
1971439734
Contributor II

I have check the format, but i still can't read back the device id, any other solutions? please

0 件の賞賛

680件の閲覧回数
syfchao
Contributor II

hello:

     I have the same problem? do you solve it ?

0 件の賞賛