Hi Team,
We are trying to integrate the NXPs TJA1101 Ethernet PHY with i.MX8MP as a 2-wire interface.
One thing to clarify is that, how can we read/write the MDIO PHY registers?
Are there any utilities available for this ?
Any help is appreciated.
Regards
Amal
I'm able to probe the driver and also set a static IP.
But when I tried to ping to another board which is of same domain, it doesn't work.
So want to read the different status and control register values. So how can we read/write these PHY registers?
Hi @jimmychan
I have cross-compiled the attached application for read the PHY registers.
Register values seems to Okay. but still the communication between tx and rx is not happening.
Link is not getting up. (LINK_STATUS register returns zero).
Whether it is the issue with dts configuration?
hi @jimmychan
&fec {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec>;
phy-mode = "rmii";
phy-handle = <ðphy1>;
fsl,magic-packet;
status = "okay";
mdio {
compatible = "fsl,nxp-tja11xx";
#address-cells = <1>;
#size-cells = <0>;
ethphy1: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
eee-broken-1000t;
rtl821x,aldps-disable;
rtl821x,clkout-disable;
};
};
};
pinctrl_fec: fecgrp {
fsl,pins = <
MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC 0x3
MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO 0x3
MX8MP_IOMUXC_SAI1_RXD4__ENET1_RGMII_RD0 0x91
MX8MP_IOMUXC_SAI1_RXD5__ENET1_RGMII_RD1 0x91
MX8MP_IOMUXC_SAI1_TXD7__ENET1_TX_ER 0x1f
MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x1f
MX8MP_IOMUXC_SAI1_TXD0__ENET1_RGMII_TD0 0x1f
MX8MP_IOMUXC_SAI1_TXD1__ENET1_RGMII_TD1 0x1f
MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x91
MX8MP_IOMUXC_SAI1_TXD6__ENET1_RX_ER 0x1f
MX8MP_IOMUXC_SAI1_MCLK__ENET1_TX_CLK 0x3
/* MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2 0x91 */
/* MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3 0x91 */
/* MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC 0x91 */
/* MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2 0x1f */
/* MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3 0x1f */
/* MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC 0x1f */
/* MX8MP_IOMUXC_SAI1_RXD0__GPIO4_IO02 0x19 */
>;
};
Hi @jimmychan
The base address of ENET in RM is typo.
The base address of fec is 0x30be0000. (you could find the correct address in dts file https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp.dtsi?...)
And read an undefined register will result in a bus error. It is better to read the register one by one.
e.g. ./memtool -32 30be0004 1 (read the EIR register)
Hi @jimmychan
We are using Linux BSP version : 5.10.35