The CAN bus consistently outputs a dominant signal, occupying the bus and preventing other nodes on the bus from sending or receiving data. At this point, CANH is at 3.7V, CANL is at 1.2V, and the ERRN pin is at a low level, indicating a continuous error. Following the instructions in the chip manual, we forcefully reset the CAN transceiver, set STB to 1, set EN to a low level to disable transceiver output. At this moment, ERRN is at a high level, resolving the error. After a period of time, we re-enable the transceiver, set EN to a high level, allowing the transceiver to output, and ERRN is also at a high level. However, CANH remains at 3.7V, CANL at 1.2V, and the error persists without recovery.
I'd like to confirm two points:
已解决! 转到解答。
Hello Ivy,
Please refer to the AN00094, Chapter 10 - Local failure diagnostics. There should be available all relevant information related to your questions. I do not have any other ANs or other documents for this pretty old CAN transceiver.
BR, Tomas
Hello Ivy,
Please refer to the AN00094, Chapter 10 - Local failure diagnostics. There should be available all relevant information related to your questions. I do not have any other ANs or other documents for this pretty old CAN transceiver.
BR, Tomas