Hello,
I'd like to indicate to the end user that the DRC (Dynamic Range Compressor) is currently active. I can't find anything that allow me to read directly in the status register anything about that. Did I miss something? In case there's no way to easily get this information, have some of you already figured out a solution to that kind of problem?
Thanks in advance,
Serge
Hello Serge,
See below. Reading bit DRC_BP (Reg0Fh[1]) you can see whether the DRC is active or bypassed.
This bit also needs to be set by the user, so it is not a status bit.
Or do you mean you would like to see whether the DRC is ON/OFF during audio playback?
So meaning a status bit that continuously toggles between 1/0 during audio playback ?
This status bit the TFA9879 does not have.
Best regards,
Tomas
PS: If this answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.