使用FS8430芯片的BULK2输出1.8V,使用TPS7A8101-Q1将1.8V换换成1.1V作为TEF8102的1.1V_FS电源,TEF8102的1.1V和1.8V供电参考验证版设计,使用PHPT60603NY,集电极采用2.3V供电,2.3V使用FS8430的BULK3产生。TEF8102的3.3V使用FS8430的LDO1产生。目前1.1V、1.8V、2.3V和3.3V都正常,FS8430的BULK2输出的1.8V也正常,只是TPS7A8101-Q1输出的1.1V_FS=0V。如果使用3.3V飞线作为TPS7A8101-Q1的输入,则会有1.1V_FS产生。