您好,TDF8532是否有可参考的驱动程序呢?
Hello.
Due to TDF8532 belongs to automotive products and without more information or documentation for public.
Please kingly contact with your local representative of NXP for more support information.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
初始化完 TDF8532, 芯片本身有自测试功能吗,输出固定频率音频?
Hello,
这个产品我们这边没有更多的资料。请联系当地的NXP进行支持。
谢谢您的理解。