Hi,
In one of my projects there is a need to use 10+ TFF1024HN in parallel which needs to give out phase aligned IF output. So my question is if I have a clock generator feeding a clock buffer/divider which is then giving out 25MHz reference to the the TFF104HN which are phase aligned and length matched will this guarantee the TFF1024HN outputs are also phase aligned.
Please refer the image for a detailed signal flow
已解决! 转到解答。
Hello,
This part number is not in our longevity program. This means we do not know exactly when it is going to be discontinued as our products are market driven.
When the product is placed in End of life, we give our customers 6-12 months for last orders and an additional 6-12 months for last shipments.
Regards.
Hello,
This part number is not in our longevity program. This means we do not know exactly when it is going to be discontinued as our products are market driven.
When the product is placed in End of life, we give our customers 6-12 months for last orders and an additional 6-12 months for last shipments.
Regards.
Hello,
Yes, you are right the TFF1024HN outputs are also phase aligned.
Please take into consideration, it is important that the LO’s of all DCV should be frequency and phase locked, if not pulling issues might rise.
Regards.