Search source flash_over_jtag_V2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Search source flash_over_jtag_V2

Jump to solution
1,028 Views
Gruenbacher
Contributor I

Hello,

I found in an other thread

http://www.freescale.com/faqdata/FAQ-19720-SRC_BCK_ALPHA21.zip

where the sourcecode from flash over jtag V2 to be found.

But the link is down (freescale???).

I Need the source to generate a new programmer for actual Windows versions, or an embedded programmer for the DSP56f803 and DSP56f8346.

From the version 1 (flash_over__jtag.exe) the source where in the SDK from motorola, but there i

get only "device busy" because this version doesn't have the "-w" option and now i must know what makes this option in the source code.

 

Had anyone the source which i can get,

thanks very much.

 

 

0 Kudos
1 Solution
1,021 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sven Grünbacher,

I attach the source code for the flash over jtag code for DSP56800E core, hope it can help you

BR

XiangJun Rong

 

View solution in original post

0 Kudos
6 Replies
7 Views
Fduch
Contributor II

And what about 56F8322 ? Is possible to use ?

 

0 Kudos
1,013 Views
Gruenbacher
Contributor I

Sorry,

but this one is not for DSP56f8346 (E core).

I need the source from FAQ 19720.

Did anyone have this FAQ?

 

Kind regard

Sven Grünbacher

 

0 Kudos
1,000 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sven,

Unfortunately, I have not the source code of flash-over-jtag for MC56F8346. As you know that the MC56F8014 uses the 56800E core, the same as that of MC56F8346.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
996 Views
Gruenbacher
Contributor I

Hallo XiangJun Rong,

thank you,

i will try it.

I look in the datasheet of 56f801 and this one is the normal core.

 

Regard

Sven Grünbacher

0 Kudos
1,022 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sven Grünbacher,

I attach the source code for the flash over jtag code for DSP56800E core, hope it can help you

BR

XiangJun Rong

 

0 Kudos
1,018 Views
Gruenbacher
Contributor I

Thank you very much,

that is what i search.

 

Kind regard

Sven Grünbacher

0 Kudos