SJA1110 mac to mac

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1110 mac to mac

263 Views
zhizhao1
Contributor I

We are trying to connect port 2 of the SJA1110 to an SOC over RGMII. 

SOC device tree:

&ethernet1 {
status = "ok";
pinctrl-0 = <&eth1_func>;
phy-mode = "rgmii";
fixed-link {
speed = <1000>;
full-duplex;
};
};

 

SJA1110 port configuration:

 

image.png

The SOC can receive network packets but cannot send them.

What is the problem with the settings?

image.png

 

Labels (1)
Tags (1)
0 Kudos
1 Reply

233 Views
abdullahzafar
NXP Employee
NXP Employee

Hi zhizhao1,

This effect usually occurs due to the clock delay not set correctly in one direction. That is the first thing that needs to be checked. I see that you are using SDK, please have a look at the snippet.

Capture.JPG

BR, 

Abdullah

 

0 Kudos