SJA1110 dynamic configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SJA1110 dynamic configuration

419件の閲覧回数
Alex_mjl
Contributor II

Hi NXP,

    I have an external S32G2 controller connected to the SJA1110. The program running in SJA1110 is a sample project "switch_config_s32g_vnp_rdb" on S32DS. The firmware "sja1110_uc.bin" for SJA1110 is loaded into sja1110 via SPI HOST. 

    Now I want to dynamically modify the configuration of SJA1110.  I would like to confirm the following questions:

    1.Is the SJA1110 register dynamically modified via the SPI_AP?

    2.Since I only loaded the firmware "sja1110_uc.bin" of sja1110, I did not load the configuration file "sja1110_switch.bin". Refer to the 5.6 summary in the UM11107.pdf, can I modify the register directly?

0 件の賞賛
返信
3 返答(返信)

352件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) yes, it can be. The SPI_AP controller offers a memory-mapped IO access into the device which allows
to control switch and some peripherals from an external microcontroller.

2) yes, you can. The “sja1110_uc.bin” is the firmware to be executed by the internal micro. When using the examples from the S32DS, the static configuration for the switch core in “sja1110_switch.bin” and “sja1110_uc.bin” is the same. So generally you don’t need the sja1110_switch.bin but only provide the sja1110_uc.bin.

BR, Petr

0 件の賞賛
返信

324件の閲覧回数
Alex_mjl
Contributor II

Thanks PetrS.

    Can you provide an example of an external microcontroller dynamically configuring L2 or Vlan via SPI_AP.

0 件の賞賛
返信

383件の閲覧回数
Alex_mjl
Contributor II

Can anyone answer that?

0 件の賞賛
返信