SJA1110 TSN CB Question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SJA1110 TSN CB Question

1,302 次查看
Ethan_L
Contributor III

Hi community,

I am testing the CB on SJA1110 and modify the example "switch_config_s32g_vnp_rdb" for testing.

I follow the CB example in document, but using DPI to identify the stream. 

If there is no redundancy between the talker and listener, they can ping without problems. as shown in the picture.

Ethan_L_1-1671764021640.png

If there is redundancy between the talker and listener, they can ping, but the icmp_seq is not continuous and sometimes takes a long time to ping. as shown in the picture.

Ethan_L_0-1671763952505.png

Is there some config I'm missing that causes these differences. The attachment is my switch configuration.

Thanks.

Ethan.

0 项奖励
回复
8 回复数

636 次查看
shanlan123
Contributor II
I follow the CB example in document

-----hello Ethan, where do you get this document.
0 项奖励
回复

1,214 次查看
nxf92355
NXP Employee
NXP Employee

Hi Ethan_L

Hope you are doing well. this case assigned to me. is any effort you done, i mean is this issue solved ? or still alive. let us know.

 

Thanks,

Tushar

 

0 项奖励
回复

1,204 次查看
Ethan_L
Contributor III

Hi @nxf92355 ,

I try to use QCI to limit the flow of broadcast storm frame. This seems to solve the problem.

I want to confirm the following,

1. Is it correct to use QCI to limit the flow of broadcast storm frames? Or is there any suggestion on avoiding broadcast storm?

2. In this CB example, whether I use QCI or not, the listener and talker cannot ping to SJA1110. Is this correct?

3. Are there more detailed usage documents and test reports about SJA1110 TSN?

Thanks,

Ethan.

0 项奖励
回复

1,140 次查看
Ethan_L
Contributor III

Hi @nxf92355 ,

Does NXP have any document and advice on broadcast storm? 

0 项奖励
回复

1,116 次查看
nxf92355
NXP Employee
NXP Employee

Hi Ethan_L

 

Hope you are doing well.

There are not such docs on nxp site. you can use NXP support to submit ticket. you can follow the below link for support

https://www.nxp.com/support/support:SUPPORTHOME

 

Regards ,

Tushar

 

0 项奖励
回复

1,113 次查看
Ethan_L
Contributor III

Hi @nxf92355 

I see. Hope NXP can add some docs and clarifications for Broadcast Storm, which I think is a basic problem for CB, and docs for TSN...

Thanks.

Ethan.

0 项奖励
回复

1,257 次查看
MayanksPatel
NXP Employee
NXP Employee

Hi @Ethan_L,

Sorry for the late.

I will be looking out on this and get back on this as soon as possible.

 

Thanks,

Mayank s Patel

1,260 次查看
Ethan_L
Contributor III

Hi community,

I think the problem is because of broadcast storm, but can't find any information about this in TSN document.

Does NXP do any config on HOST or SJA1110 to avoid broadcast storm in CB example?

Or any advice on avoiding broadcast storm?

Thanks.

Ethan.

0 项奖励
回复