[SJA1110] SPI driver can not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[SJA1110] SPI driver can not work

1,501件の閲覧回数
Ethan_L
Contributor III

Hi everyone,

I am a software RD who's working on SJA1110 ethernet switch project.

I am testing the SPI driver on SJA1110, but I can not measure any signal on the oscilloscope even in master or slave mode.

Does anybody have an idea for this?

Is there any example or document about how to use SPI driver?

 

Thanks, Ethan.

0 件の賞賛
返信
7 返答(返信)

833件の閲覧回数
Edieyeee
Contributor I

Hello Ethan,have you solve this problem?

0 件の賞賛
返信

1,451件の閲覧回数
kaden
NXP Employee
NXP Employee

Hi Ethan_L, 

so you want to try to configure the switch via SPI from S32G? Did you check the DIP switch settings are in the correct position? 

They should be set to Serial Boot. 

BR

Kevin

0 件の賞賛
返信

1,433件の閲覧回数
Ethan_L
Contributor III

Hi Kevin,

I set the DIP switch to serial boot mode, but still can't measure any signal.(resistance R607, R624)

Is there any example or document about spi?

Thanks,

Ethan.

0 件の賞賛
返信

1,478件の閲覧回数
kaden
NXP Employee
NXP Employee

Hi Ethan_L,

can you provide additional information? Which hardware are you using (NXP reference board or own design), which software (SJA1110SDK)?

BR

Kevin

0 件の賞賛
返信

1,470件の閲覧回数
Ethan_L
Contributor III

Hi Kevin,

I use S32G-VNP-RDB2 EVM and SDK is SJA1110_SDK(version 1.0.1).

I modified the example "switch_config_s32g_vnp_rdb" for testing.

I try to make S32G274 and SJA1110 communicate via SPI, but it doesn't work.

 

Thanks,

Ethan.

0 件の賞賛
返信

526件の閲覧回数
Haribadri1989
Contributor II
Hi Ethan, have you solved this problem?
0 件の賞賛
返信

982件の閲覧回数
shanlan123
Contributor II
Hi Ethan_L, have you solve this problem?
0 件の賞賛
返信