[SJA1110] SPI driver can not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[SJA1110] SPI driver can not work

1,342 次查看
Ethan_L
Contributor III

Hi everyone,

I am a software RD who's working on SJA1110 ethernet switch project.

I am testing the SPI driver on SJA1110, but I can not measure any signal on the oscilloscope even in master or slave mode.

Does anybody have an idea for this?

Is there any example or document about how to use SPI driver?

 

Thanks, Ethan.

0 项奖励
回复
7 回复数

674 次查看
Edieyeee
Contributor I

Hello Ethan,have you solve this problem?

0 项奖励
回复

1,292 次查看
kaden
NXP Employee
NXP Employee

Hi Ethan_L, 

so you want to try to configure the switch via SPI from S32G? Did you check the DIP switch settings are in the correct position? 

They should be set to Serial Boot. 

BR

Kevin

0 项奖励
回复

1,274 次查看
Ethan_L
Contributor III

Hi Kevin,

I set the DIP switch to serial boot mode, but still can't measure any signal.(resistance R607, R624)

Is there any example or document about spi?

Thanks,

Ethan.

0 项奖励
回复

1,319 次查看
kaden
NXP Employee
NXP Employee

Hi Ethan_L,

can you provide additional information? Which hardware are you using (NXP reference board or own design), which software (SJA1110SDK)?

BR

Kevin

0 项奖励
回复

1,311 次查看
Ethan_L
Contributor III

Hi Kevin,

I use S32G-VNP-RDB2 EVM and SDK is SJA1110_SDK(version 1.0.1).

I modified the example "switch_config_s32g_vnp_rdb" for testing.

I try to make S32G274 and SJA1110 communicate via SPI, but it doesn't work.

 

Thanks,

Ethan.

0 项奖励
回复

367 次查看
Haribadri1989
Contributor II
Hi Ethan, have you solved this problem?
0 项奖励
回复

823 次查看
shanlan123
Contributor II
Hi Ethan_L, have you solve this problem?
0 项奖励
回复