SJA1110 SGMII MAC to MAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1110 SGMII MAC to MAC

694 Views
lance3
Contributor I

Can someone confirm if the SJA1110 SGMII 2.5Gbps can be used in MAC to MAC mode? I am looking at connecting two SJA1110A back-to-back with the SGMII as the interconnect with fixed speed of 2.5Gbps. 

Thanks,

0 Kudos
4 Replies

581 Views
MateoSegura413
Contributor III

Hello, is this MAC to MAC connection only possible on the SGMII ports? 

We are trying to connect port 2 of the SJA1110 to an MCU over RMII. (without a PHY) on the same PCB. We hooked up a REF_CLK at 25Mhz and setup the MCU to use this clock since it's usually the PHY providing this. 

Is this even possible? We've tried all the possible configurations on that port and no luck. 

MateoSegura413_0-1671732560556.png

 

Any help and guidance is greatly appreciated.

0 Kudos

389 Views
shanlan123
Contributor II
have you solve this problem?
0 Kudos

671 Views
lance3
Contributor I

Hi @kaden , many thanks - exactly the information I was after. 

0 Kudos

677 Views
kaden
NXP Employee
NXP Employee

Hi @lance3 ,

yes, it is possible to cascade two SJA1110 with the 2.5G SGMII interfaces. There is also an SJA1110 evaluation board with the exact same use case:

https://www.nxp.com/products/interfaces/ethernet-/automotive-ethernet-switches/sja1110-evm-evaluatio...

Best regards

Kevin