SJA1105Q short two pins/ Config via JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SJA1105Q short two pins/ Config via JTAG

477件の閲覧回数
BravoEven
Contributor I

Hello:

    Are there any risk to short the SPI input and the RX_DV of port0 ? I have a mistake of HW design so I have to short the two pins.

     I have tried once but the transmission of other ports does not work. So I break the connection. 

     By the way , can we config the SJA1105Q via Jtag interface? Then I will not need to take a risk to short two pins above.

     Thanks!

タグ(1)
0 件の賞賛
返信
2 返答(返信)

474件の閲覧回数
BravoEven
Contributor I
sorry it is the TX_EN of port0 but not RX_DV!
0 件の賞賛
返信

461件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Unfortunately you can't short SPI port to others pin and Jtag can't be used in SJA1105 which is not the MCU or processor.

0 件の賞賛
返信