Hello,
I am trying to use a SJA1105Q switch connected to an i.MX8QM processor (on port 4) and to three Broadcom PHYs (on ports 0-1-2). I am using Linux 5.10.71 as found in i.MX SDK release Linux 5.15.71_2.2.1, and the SJA1105 driver included in the kernel.
I set up a bridge using systemd (but I also tried manually) to be able to use the switch in "bridge mode", as indicated in https://docs.kernel.org/networking/dsa/configuration.html
I am however not able to communicate neither from my board to an external entity nor between entities connected to two ports of the switch.
Here is my configuration:
devicetree
&fec1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec1>;
/* Clock delay on TXC and RXC lines are applied at switch side */
phy-mode = "rgmii-id";
nvmem-cells = <&fec_mac0>;
nvmem-cell-names = "mac-address";
phy-reset-gpios = <&lsio_gpio0 26 GPIO_ACTIVE_HIGH>;
phy-reset-duration = <1>;
phy-reset-post-delay = <1>;
mdio {
#address-cells = <1>;
#size-cells = <0>;
fec1_phy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c45";
reg = <0>;
};
fec1_phy1: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c45";
reg = <1>;
};
};
fixed-link {
speed = <1000>;
full-duplex;
};
};
&lpspi0 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi0 &pinctrl_lpspi0_cs>;
status = "okay";
cs-gpios = <&lsio_gpio3 5 GPIO_ACTIVE_LOW>;
sja1105: ethernet-switch@0 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eth_hub>;
compatible = "nxp,sja1105q";
#address-cells = <1>;
#size-cells = <0>;
reg = <0>;
spi-max-frequency = <12000000>;
/* Sample data on trailing clock edge */
spi-cpha;
/* SPI controller settings for SJA1105 timing requirements */
fsl,spi-cs-sck-delay = <1000>;
fsl,spi-sck-cs-delay = <1000>;
/* Driver reset logic is inverted - fix it with GPIO_ACTIVE_LOW here */
reset-gpios = <&lsio_gpio0 16 GPIO_ACTIVE_LOW>;
sja1105,startup-delay = <5>;
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
label = "swp0";
phy-handle = <&fec1_phy0>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <0>;
};
port@1 {
label = "swp1";
phy-handle = <&fec1_phy1>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <1>;
};
port@2 {
label = "swp2";
phy-handle = <&fec2_phy0>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <2>;
};
port@4 {
ethernet = <&fec1>;
/* Clock delays are applied by the SJA1105 */
phy-mode = "rgmii-id";
reg = <4>;
fixed-link {
speed = <1000>;
full-duplex;
};
};
};
};
};
br0.netdev
[NetDev]
Name=br0
Kind=bridge
br0.network
[Match]
Name=br0
[Network]
Address=192.168.0.2/24
swp.network
[Match]
Name=swp*
[Network]
BindCarrier=eth0
Bridge=br0
ConfigureWithoutCarrier=yes
Output of ip addr
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
inet 127.0.0.1/8 scope host lo
valid_lft forever preferred_lft forever
inet6 ::1/128 scope host
valid_lft forever preferred_lft forever
2: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1504 qdisc mq state UP group default qlen 1000
link/ether ba:01:11:86:31:72 brd ff:ff:ff:ff:ff:ff
inet6 fe80::b801:11ff:fe86:3172/64 scope link
valid_lft forever preferred_lft forever
3: eth1: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc mq state DOWN group default qlen 1000
link/ether ea:23:fd:7f:ac:e2 brd ff:ff:ff:ff:ff:ff
inet 192.168.0.2/24 brd 192.168.0.255 scope global eth1
valid_lft forever preferred_lft forever
4: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UP group default qlen 10
link/can
5: can1: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UP group default qlen 10
link/can
6: swp0@eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc noqueue master br0 state UP group default qlen 1000
link/ether ba:01:11:86:31:72 brd ff:ff:ff:ff:ff:ff
7: swp1@eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc noqueue master br0 state UP group default qlen 1000
link/ether ba:01:11:86:31:72 brd ff:ff:ff:ff:ff:ff
8: swp2@eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc noqueue master br0 state UP group default qlen 1000
link/ether ba:01:11:86:31:72 brd ff:ff:ff:ff:ff:ff
9: can2: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UP group default qlen 10
link/can
10: usb0: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc pfifo_fast state DOWN group default qlen 1000
link/ether 12:0c:32:b5:90:87 brd ff:ff:ff:ff:ff:ff
11: br0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc noqueue state UP group default qlen 1000
link/ether ba:01:11:86:31:72 brd ff:ff:ff:ff:ff:ff
inet 172.16.0.100/12 brd 172.31.255.255 scope global br0
valid_lft forever preferred_lft forever
inet6 fe80::dcd9:3aff:fec2:1ec8/64 scope link
valid_lft forever preferred_lft forever
Output of bridge link
6: swp0@eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 master br0 state forwarding priority 32 cost 4
7: swp1@eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 master br0 state forwarding priority 32 cost 19
8: swp2@eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 master br0 state forwarding priority 32 cost 19
Do you have any idea on why this is happening?
Thank you very much in advance
Kind regards,
Francesco Valla
Solved! Go to Solution.
Dear @brian14 (and all other concerned parties),
I found the issue to be an incorrect configuration of the RGMII delays inside the driver of the PHY, so not really an issue of the SJA1105Q.
As a reference, my final DTS configuration is the following one (in the end, I decided to apply RGMII delays at SoC and PHYs side):
&fec1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec1>;
/* Clock delay on TXC and RXC lines are applied at FEC side by the
* fsl,rgmii_*xc_dly properties below */
phy-mode = "rgmii";
fsl,rgmii_rxc_dly;
fsl,rgmii_txc_dly;
nvmem-cells = <&fec_mac0>;
nvmem-cell-names = "mac-address";
phy-reset-gpios = <&lsio_gpio0 26 GPIO_ACTIVE_HIGH>;
phy-reset-duration = <1>;
phy-reset-post-delay = <1>;
mdio {
#address-cells = <1>;
#size-cells = <0>;
fec1_phy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c45";
reg = <0>;
};
fec1_phy1: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c45";
reg = <1>;
};
};
fixed-link {
speed = <1000>;
full-duplex;
};
};
&lpspi0 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi0 &pinctrl_lpspi0_cs>;
status = "okay";
cs-gpios = <&lsio_gpio3 5 GPIO_ACTIVE_LOW>;
sja1105: ethernet-switch@0 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eth_hub>;
compatible = "nxp,sja1105q";
#address-cells = <1>;
#size-cells = <0>;
reg = <0>;
spi-max-frequency = <12000000>;
/* Sample data on trailing clock edge */
spi-cpha;
/* SPI controller settings for SJA1105 timing requirements */
fsl,spi-cs-sck-delay = <1000>;
fsl,spi-sck-cs-delay = <1000>;
/* Driver reset logic is inverted - fix it with GPIO_ACTIVE_LOW here */
reset-gpios = <&lsio_gpio0 16 GPIO_ACTIVE_LOW>;
sja1105,startup-delay = <5>;
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
label = "swp0";
phy-handle = <&fec1_phy0>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <0>;
};
port@1 {
label = "swp1";
phy-handle = <&fec1_phy1>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <1>;
};
port@2 {
label = "swp2";
phy-handle = <&fec2_phy0>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <2>;
};
port@4 {
ethernet = <&fec1>;
/* Clock delays are applied by the SoC */
phy-mode = "rgmii";
reg = <4>;
fixed-link {
speed = <1000>;
full-duplex;
};
};
};
};
};
Dear @brian14 (and all other concerned parties),
I found the issue to be an incorrect configuration of the RGMII delays inside the driver of the PHY, so not really an issue of the SJA1105Q.
As a reference, my final DTS configuration is the following one (in the end, I decided to apply RGMII delays at SoC and PHYs side):
&fec1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec1>;
/* Clock delay on TXC and RXC lines are applied at FEC side by the
* fsl,rgmii_*xc_dly properties below */
phy-mode = "rgmii";
fsl,rgmii_rxc_dly;
fsl,rgmii_txc_dly;
nvmem-cells = <&fec_mac0>;
nvmem-cell-names = "mac-address";
phy-reset-gpios = <&lsio_gpio0 26 GPIO_ACTIVE_HIGH>;
phy-reset-duration = <1>;
phy-reset-post-delay = <1>;
mdio {
#address-cells = <1>;
#size-cells = <0>;
fec1_phy0: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c45";
reg = <0>;
};
fec1_phy1: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c45";
reg = <1>;
};
};
fixed-link {
speed = <1000>;
full-duplex;
};
};
&lpspi0 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi0 &pinctrl_lpspi0_cs>;
status = "okay";
cs-gpios = <&lsio_gpio3 5 GPIO_ACTIVE_LOW>;
sja1105: ethernet-switch@0 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eth_hub>;
compatible = "nxp,sja1105q";
#address-cells = <1>;
#size-cells = <0>;
reg = <0>;
spi-max-frequency = <12000000>;
/* Sample data on trailing clock edge */
spi-cpha;
/* SPI controller settings for SJA1105 timing requirements */
fsl,spi-cs-sck-delay = <1000>;
fsl,spi-sck-cs-delay = <1000>;
/* Driver reset logic is inverted - fix it with GPIO_ACTIVE_LOW here */
reset-gpios = <&lsio_gpio0 16 GPIO_ACTIVE_LOW>;
sja1105,startup-delay = <5>;
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
label = "swp0";
phy-handle = <&fec1_phy0>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <0>;
};
port@1 {
label = "swp1";
phy-handle = <&fec1_phy1>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <1>;
};
port@2 {
label = "swp2";
phy-handle = <&fec2_phy0>;
/* Clock delays are applied by the external PHY */
phy-mode = "rgmii-id";
reg = <2>;
};
port@4 {
ethernet = <&fec1>;
/* Clock delays are applied by the SoC */
phy-mode = "rgmii";
reg = <4>;
fixed-link {
speed = <1000>;
full-duplex;
};
};
};
};
};
Thank you for contacting NXP Support and for your detailed information.
I have reviewed your configurations, and it seems that they are correct.
However, I think you can use a similar debugging process described by a colleague on the following thread:
The four phys connected to sja1105Q cannot be load... - NXP Community
Have a great day!