SJA1105 时间戳

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1105 时间戳

452 Views
BravoEven
Contributor I

您好,我想通过SJA1105配置时间戳功能,但是使用过滤模式时如果使用

MAC_FLTRES[0]阈值的地址作为目的地址,则似乎会被丢弃,也没有等到META帧,对应设置如下,请问是其他地方还需要设置吗?另一种TCAM设置转发规则我也没搞通,痛苦,,求解惑!谢谢
BravoEven_0-1682068803818.png

 

0 Kudos
2 Replies

424 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @BravoEven 

In order to use timestamping, it's necessary to use frame trapping (this is explained in more detail in the AH1704 (7.3 Timestamping and AVB).
https://www.nxp.com/webapp/Download?colCode=AH1704&location=null

Also please read chapter 7.3.3 1-step and 2-step SYNC frames.
An example for gPTP can be found in chapter 7.6.6 of the respective application hints.

Regards,

Lukas

0 Kudos

391 Views
BravoEven
Contributor I

Hello 

      now I want to take the egress timestamp of frame to the host port, for example, a PTP sync frame is forwarded from port1 to port0(host port), I can get the ingress time stamp by the META frame, but how can i get the egress timestamp to calculate the resident time?

0 Kudos