Hello,
I'm using an SE050 with an ESP32S3. I want to upgrade esp-idf version to 5.2.1 but I've some problem with mdbedtls.
In your Plug & Trust middleware, mbedtls used version is 2.28.3.
In esp-idf version, mbedtls used version is 3.5.2.
Do you plan to update your middleware to be compatible with mdebtls 3.x.x ?
Thank you
Hi @jb2 ,
Actually it depends on SDK team's schedule , when the platforms supported by MW have a updated mbedtls version in SDK mainstream , there will be changes in MW as well.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------