Hello team.
I am currently configuring SBC_FS26 using EB Tresos. While reading the RTD_SBC_FS26_IM.PDF manual:
I came across a statement that says, "The Sbc_fs26 driver was designed to be configured by using the EB Tresos Studio (version 29.0.0 or later)." Does this mean that I absolutely have to use EB Tresos version 29.0.0 or later?
However, I am currently using EB Tresos version 28.0.2, which can also open the configuration of SBC_FS26.
I would like to know what the differences are between configuring SBC_FS26 using these two versions of EB Tresos.
Thanks
Hello Shi,
I suppose you can use a different version, but we cannot confirm the integrity.
The entire development and tests took place on 29.0, so it is hard to say whether everything will work 100%.
BR, Tomas